Part Number: TMS320F28P650SH
Other Parts Discussed in Thread: F29H850TU
I installed CCS 2.5.0 today (Mac edition) - I was running 2.4.0, and I agreed to the automatic update. Now, when I initiate a debug session, the all-too-familiar "Reconnecting to TI Cloud Agent" popup appears. Whereas this message was previously very annoying, it now happens EVERY time I initiate a debug session, and it makes it impossible for me to connect to my target.
So I am now effectively dead-in-the-water, which is why I consider this a catastrophic bug. I obviously need this to be fixed quickly.
Going back to 2.4.0? Not an option, apparently, since I selected the automatic update.
Wiping CCS and starting over with 2.4.0 seems to be my only option, which would mean wiping out all of my settings. If you can tell me a way to save those settings and restore them on a new install, that would be helpful too.