I am trying run the FFTC_Simple_testProject that comes with MCSDK 2_00_05_17 on a C6670. The instructions in the Readme.txt state: 'run the multi core example project
on all 4 cores in "synchronous" mode.' I am using CCSv5.1. These instructions seem to be for CCSv4. I think the CCSv5 equivalent is to group the cores as per [http://processors.wiki.ti.com/index.php/Multi-Core_Debug_with_CCSv5#Fixed_Groups]. However when I select multiple cores and right click the context menu I get is quite different. See the attached screenshot. I have not modified the example code nor the configuration file. It makes no difference whether I select main(), _c_int00() or the core names.