Hello,
I had to reinstall the CCS. No I'm not able to get the System Analyzer via Tools -> System Analyzer in the Debug View.
Setup is as follows:
-OS is Windows 7
-CCS 5.1.0.09000
-Bios MCSDK 2_00_05_17 installed
I've checked the following things:
-In CCS -> Help -> About -> Installation Details -> Installed Software -> UIA 1.0.3.25 is installed
-Trying the Tutorial 1 for SystemAnalyzer:
-Checked UIA-Target for XDC-Tools in Products and Repositories
-Used Target elf.C66 and Platform evm6678 and Build-profile Debug
Using the Tutorial or my own example, I'm not able to get the System Analyzer; before reinstalling CCS, everything worked fine.
Thanks for help,
Best Regards,
Bernd