This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

running ccsv5 simulator on command prompt

Hello,

I want to run my application on c64x+ simulator using command prompt .

Can anyone please tell me the procedure for this. How to pass .ccxml file as argument to  simulator?

Regards,

Mike

  • Mike,

    I would suggest checking out loadti.  This is an example debug server script that acts as a command line loader.

    This example is included with CCS.

    http://processors.wiki.ti.com/index.php/Loadti

    Regards,

    John

  • Hello John,

    Thank you very much for your reply.

    I will try this at my end.

    Regards,

    Mike

  • I just downloaded a "fresh" ccs5 (CCS5.2.0.00069_linux.tar.gz)

    followed instructions on the link you provided, and get this error:

    Mandatory arguments to long options are mandatory for short options too.

    did it get broken?

  • What is the command line you are using to run loadti?

  • I've tried a bunch...

    I have my own wrapper script:

    P=ccsv5/ccs_base/scripting/examples
    C=ccsv5/ccs_base/common/targetdb/configurations

    PATH=$CCSV5BASE/$P/loadti:$PATH

    app=test_prog.out

    # same error out of all of these:

    loadti.sh -q --cfg-file=$CCSV5BASE/$C/tisim_c64xple.xml $app

    loadti.sh -q -c=$CCSV5BASE/$C/tisim_c64xple.xml $app

    loadti.sh -q -c $CCSV5BASE/$C/tisim_c64xple.xml $app

    loadti.sh -q -c $CCSV5BASE/$P/TestServer/c64xp_le_sim.ccxml $app

  • I see this issue also. I'm taking a look at this and will post any updates as I find more details...

  • Any command-line arguments to the shell script are not getting passed to the main loadti javascript (main.js). Most likely some bug with the shell scripts. Still under investigation...

  • I munged through the several layers of shell scripts and came up with this single script... (it got me further but still fails)

    $ cat sim

    #!/bin/ksh

    export CCSV5BASE=/opt/TI

    export B=ccsv5/ccs_base
    export R=$B/scripting
    export C=$B/common/targetdb/configurations
    export P=$R/examples

    DEBUGSERVER_ROOT=$CCSV5BASE/$B/DebugServer
    export DEBUGSERVER_ROOT

    CLASSPATH=$DEBUGSERVER_ROOT/packages/ti/dss/java/js.jar:$CLASSPATH
    CLASSPATH=$DEBUGSERVER_ROOT/packages/ti/dss/java/dss.jar:$CLASSPATH
    CLASSPATH=$CCSV5BASE/$B/dvt/scripting/dvt_scripting.jar:$CLASSPATH
    export CLASSPATH

    export JAVA_HOME=$CCSV5BASE/ccsv5/eclipse/jre
    PATH=$JAVA_HOME/bin:$PATH

    export LOADTI_PATH=$CCSV5BASE/$P/loadti

    java -DXPCOM.RUNTIME=$DEBUGSERVER_ROOT/linux org.mozilla.javascript.tools.shell.Main $CCSV5BASE/$P/loadti/main.js -c $CCSV5BASE/$P/TestServer/c64xp_le_sim.ccxml test_layout

    $ ./sim

    ***** DSS Generic Loader *****

    START: 15:46:39 GMT-0700 (MST)

    Configuring Debug Server for specified target...
    Done
    flxInitLoad: client has not been protected.
    flxInitLoad: client has not been protected.
    TARGET: C64x+ CPU Cycle Accurate Simulator, Little Endian_0
    Connecting to target...
    testEnv.outFiles: test_layout
    Loading test_layout
    #
    # An unexpected error has been detected by Java Runtime Environment:
    #
    # SIGSEGV (0xb) at pc=0x0026f666, pid=24376, tid=1811778416
    #
    # Java VM: Java HotSpot(TM) Server VM (11.3-b02 mixed mode linux-x86)
    # Problematic frame:
    # C [libc.so.6+0x7e666]
    #
    # An error report file with more information is saved as:
    # /tmp/hs_err_pid24376.log
    #
    # If you would like to submit a bug report, please visit:
    # http://java.sun.com/webapps/bugreport/crash.jsp
    # The crash happened outside the Java Virtual Machine in native code.
    # See problematic frame for where to report the bug.
    #
    Abort

    I can send the .log file if you'd like it

  • is my quickest path to simulator functionality to DL an older release?

  • dkerns said:
    I can send the .log file if you'd like it

    log and dmp files would be great. If you can also provide the test_layout executable, that;d be great too.

    http://processors.wiki.ti.com/index.php/Troubleshooting_CCSv5#CCS_Diagnostic_Logs

    Thanks

    ki

  • in my profile

  • as another data point, I downloaded the previous release (CCS5.1.1.00033) and get the same error.

  • for both versions (CCS5.1.1.00033 and CCS5.2.0.00069) I never did the admin driver step... could that be causing my errors? (I've never attempted to start CCS5 gui, only tried running the simulator from the command line) ... Do I need to start a new thread for this issue? (since this one is marked solved)

  • dkerns said:
    for both versions (CCS5.1.1.00033 and CCS5.2.0.00069) I never did the admin driver step... could that be causing my errors?

    oh.. did you install as root? If not, then there would be an issue. If you did install as root, you don't need to do the extra step of running the script for the emulation drivers.

    dkerns said:
    Do I need to start a new thread for this issue? (since this one is marked solved)

    I'll split this thread to a new thread

    ki

  • last night I got on a lab machine (where I have root) and installed CCS5.2.0.00069 as root.

    the c6000 simulator still get the same error.