I am trying to setup profiling of a C routine running on the EVM board, to collect CPU cycle stats for the routine.
According to CCS help, I have to activate Trace Analyzer>Open or Trace Analyzer>connect to, and then setup profiling via Trace Analyzer>Profiling etc.
The problem that I have is my Trace Analyzer Open Connection menu is disabled.. Is this because I am using 90-day evaluation version of the CCS, or am I missing certain BIOS/RTDX/RTA etc. packages? What do I need to do profiling?
Thanks in advance!
Fernando