This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UNIFLASH: Using CLI interface to read device's unique id back

Part Number: UNIFLASH

Hi expert,

We now have a customer request to use UNIFLASH Command Line Interface to read back the device unique id for datalog.

Is there any method to read a certain value from flash address and overwrite to a certain file (like .txt file)?

I see there supports to use read command with certain flash address range, while this can only been used to create a firmware.bin file.

I would like to ask if there any other method to achieve this customer request with CLI interface.

Thanks for your support!

B.R.

Sal