This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to profile code for C6748

Other Parts Discussed in Thread: OMAP-L138, CCSTUDIO

Hi,

I am running some test code on C6748 (using a OMAP-L138 eval board from Logic PD. I am using the DSP module only and not the module with ARM + C6748).

The board is hooked up to the host machine through a XDSv2 USB emulator and the 14-pin TI connector.

I need to profile the code to understand bottlenecks better. But, when I click on "Profile -> Setup", I do not get options to enable different profiling options.

Is there a way to profile code running on C6748 using CCStudio v5?

Thanks,

-raja.