Champs,
Could any one help to confirm whether Blackhawk 560PCI emulatore could works under 32bit win7? The driver is together with the CCS4.x or CCS5.1, or any place to get the update drivers?
best regards,
David
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Champs,
Could any one help to confirm whether Blackhawk 560PCI emulatore could works under 32bit win7? The driver is together with the CCS4.x or CCS5.1, or any place to get the update drivers?
best regards,
David
Hi David,
DBian said:Could any one help to confirm whether Blackhawk 560PCI emulatore could works under 32bit win7?
Yes, it is supported.
DBian said:The driver is together with the CCS4.x or CCS5.1, or any place to get the update drivers?
Blackhawk drivers come with CCSv4 and v5.
Thanks
ki