This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CODECOMPOSER: Hex file generation

Part Number: CODECOMPOSER
Other Parts Discussed in Thread: TMS570LS0914

Hello,

I am using Code Composer Studio (CCS) Version 12.2.0.00009 for software development on both TMS570 and TMS320 series microcontrollers.

When I flash the hex file generated from CCS onto the device using the bootloader, the flashing process completes successfully. However, the application does not run as expected afterward.

In contrast, when I flash or debug the same code directly through CCS, it executes correctly without any issues. 

The hex utility settings are as below :

image.png

Kindly help me to get it resolved.

Thanks,

Prajakta