This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CODECOMPOSER: Recurrent Git (built-in) extension error "Right-hand side of 'instanceof is not an object"

Part Number: CODECOMPOSER

When using the Git (built-in) `v1.95.3` extension in Code Compose Studio v20.5.1.12 a pop-up error window apperas when attempting any major git operation. The content of this error window is:

Git: Right-hand side of 'instanceof is not an object

That said all operations complete succesfully and no errors are present neither in the Git Log nor in the CCS Developer Tools Console.

Plaing around with the Git extension folder settings I've found out that this issue is present only when the option Close Diff On Operation is set to true.
That said I've also found out that, at least once, the first time the Close Diff On Operation action will attempt to execute with at least one open Diff tab the recurrent issue can be solved permanently! I've attempted to repeat the steps listed above but the recurrent error is now not disappering, and I have to set Close Diff On Operation is set to false to solve the issue.