This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6748: Code Composer Install

Part Number: TMS320C6748

I am attempting to install Code Composer v6.1.3. When I try to install via the .exe file, I go through the entire setup process with no issues, but it then fails during the install. I'm getting the error message: "Warning : MSVC components failed to install. Please install executables manually from C:/ti/ccsv6/installers before using CCS". When I go to that folder, the only file in there is "vcredist_x86_2015_14.0.23506.exe" which I also cannot install as I have a newer version of Visual Studio installed on my machine. How can I remedy this without uninstalling my current Visual Studio version?