Hello Folks
this is regarding the drivers for beaglebone on windows 7 x64. I am having problems getting the bone connected to my host. I tried installing the 64bit drivers provided on the beagleboard website but it looks like they are broken (as was confirmed from a quick google search). So on further probing, came across different methods to get it working. One of the guys mentioned that the drivers provided with CCSv5.1 also work fine for the bone.
In his own words: "I have previously installed Code Composer Studio, which installed the XDS100v2 drivers onto my system. It so happens that these are the drivers with the correct VID/PID for the FTDI chip on the Beaglebone. When I connect the Bone, the XDS100v2 drivers are the ones that load, followed by a USB-serial driver". But for me, even after installing the CCSv5.1, I am not able to get the beaglebone connected to my laptop which is a windows 7 x64 machine. I would appreciate if someone was able to get the bone to connect to a windows 7 x64 machine using the drivers provided with the CCSv5.1 . Furthermore, methods to get the bone connected to the machine outside of CCSv5.1 are also welcome.
Keen to hear from you folks