Hi,
We are using CCSv5 with a Spectrun Digital XDS560v2 STM and would like to be able to monitor L3 transactions.
In the OMAP4430 TRM section '1.3.9 On-Chip Debug Support Description' states that
OCP watch-point (OCP-WP):
• Monitors L3 interconnect transaction when target transaction attributes match the user-defined
attributes or trigger on external debug event
But we have not found that any trace data is coming from the OCP-WP when we select it under the Breakpoint-Trace menu.
We have been able to get Performance Probe data through the STM; so the connection to the STM block on the target is good.
Is there a Gel file or script that needs to be configured to turn on the L3 data?
Thank you,
Bruce.