Other Parts Discussed in Thread: SYSBIOS
Hi, I have just upgraded CCS from V5.1.0.09000 to V5.1.1.00028. When I load my previous projects in the new CCS v5.1.1, several red error indicators show up in the Project Explorer (see attached). I did a "Clean Project" and a "Build Project" to every project that has the red error indicator. The builds were successful but the red error indicators stayed on. They do not affect build and debug but it is annoying to see them there. Is there any way to get rid of those red error indicators? Thanks, Zhao