Hi,
I am using CCS 5.1.0.04001 and trying to connect to the EVM6424. I am launching the new target configuration and choosing the connection spectrum digital DSK-EVM_eZdsp onboard USB Emulator and device EVM6424. When i am trying to debug and connect the target i am getting the error message as
C64XP_0: GEL Output:
EVM6424 Startup Sequence
C64XP_0: GEL Output: Setup CacheC64XP_0: GEL: Error while executing OnTargetConnect(): Driver did not attempt to write memory at 0x01845028.
The same is working in CCSV3.3 and in CCS5 i am not able to connect and load the GEL file. Please help.
Thank You