This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSTUDIO-THEIA: Removed workspace folder is recreated on next CCStudio startup

Part Number: CCSTUDIO-THEIA
Other Parts Discussed in Thread: CCSTUDIO

Really a not so problematic issue observed when investigating the "related" issue in a temporary workspace.

  • Close CCStudio after working in workspace "temp"
  • Delete the workspace folder "temp" in Windows
  • Restart CCStudio
    • It tries to reopen the removed workspace, and recreates the "temp" folder in its original location. Empty.

Fun fact: I have none of the AI agents activated that are now supported in this CCS version. They might have guessed whether the "temp" meant "temporary" and skip trying to reopen it, or "temperatureAnalysis" and not only recreate the folder, but also a reasonable contents that you might expect there.

I guess the observed behaviour is often a feature (wanted behaviour) and not a bug (unwanted behaviour). But a notification would be nice.

  • I guess the observed behaviour is often a feature (wanted behaviour) and not a bug (unwanted behaviour). But a notification would be nice.

    Yes, this is expected behavior. CCS will remember the location of the last workspace used and if it doesn't exist, it will re-create the folder and use it.

    For a fresh install, it will use the default ~/workspace_ccstheia and create it if it doesn't exist and use it.

    What type of notification are you looking for? Something like "folder <name> doesn't exist, creating new one"?

  • Indeed.

    I guess that apart from the fresh install situation, each time that the last workspace has 'disappeared' when starting CCS is worth a notification. Either you have deliberately deleted it yourself (my use case this time), in which case it is handy to know that the folder is recreated.

    Or, the folder has gone missing unintended, in which case a notification is even more useful. In both cases, it is (usually/hopefully) a rare event: help or guidance of your tool is than most welcome.