This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

${inputs} linker order



My apologies if this has already been asked elsewhere.

I've run into an issue using the linker in CCSv5 (using version 5.1.0.09000).  In my build configuration, when I select the "TMS470 Linker", it shows the command line options (currently looks something like ${command} ${flags} ${output_flag} ${output} ${inputs}).  The ${inputs} tag seems to include all of the object and library files found in the project.

My issue is with respect to the order in which this automatic list is generated.  My situation involves both compiling a project locally, and packaging up all the object files into a library archive to be compiled elsewhere.  This seems to work fine for the most part - but an issue arises when compiling on the remote machine (from the library archive).  The build process involves including other libraries (with the "-l" tag).  One of these libraries defines a symbol that is already defined in my local libraries.

This is fine locally - the ${inputs} lists my own object files first, then includes the "-l" for the supplementary library file.  Remotely, however, the "-l" link is included before my own library file.

I can fix this issue by removing the library file from the "File Search Path" list of included libraries and including it manually on the command line (in the "TMS470 Linker" menu, so the command line now looks like ${command} ${flags} ${output_flag} ${output} ${inputs} -l"otherlibfile.lib").

Is there any way to configure the order that files are included in the ${inputs} tag, or do I have to do it manually on the command line?

  • Hi Owen,

    If you go to the project properties (Project -> Properties) and then select 'Build' in the left panel and then the 'Link Order' tab in the right panel, you can specify the link order. I believe this what you are looking for?

    Thanks

    ki

  • Hi Ki,

    Thanks for your response.  This does allow me to pick the order in which the libraries are linked.

    I don't know whether this forum or thread is the appropriate venue for feature suggestions, but it may be useful to have an option within the "Link Order" tab that includes everything else.  Right now, I can pick off every item from the list and organize them all individually, but the order for most of them doesn't matter - just a select few.  Right now, if I pick only three or four items from the list, it appends all the others at the end.  It may be helpful to have an "Everything Else" item, so that I could pick off a few items, have some includes specifically at the beginning, some at the end, and "Everything Else" in between.  So my link order would look like

    • -l"startinglibrary.lib"
    • "$(EVERYTHING_ELSE)"
    • -l"endlinglib1.lib"
    • "LinkerCommandFile.cmd"
    • -l'"endinglib2.lib"

    I did notice a "$(GEN_CMDS_QUOTED)" option, but it does not appear to include anything.  Do you happen to know what this is meant for?

    Thanks,

    Owen