This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C2000WARE: Print program listing.

Part Number: C2000WARE

Is there a way to print a C2000ware program listing that has been loaded into CCS V21?  I tried copy and paste but it either presents as a solid block or loses color coding and format.  (Earlier CCS versions had a File print option that worked well.)

  • Sorry I didnt understand can you please clarify what you want to achieve?

  • I just want to print a readable listing of the source of any program that has been loaded into CCS V21.  As noted, copy and paste introduces substantial distortions in the printed output versus what is on the screen.  The File -> Print option available in earlier versions of CCS does not seem to be available.  Is this feature or an equivalent accessable in some other way?

  • Hi Gary,

    There are 2 ways

    1. Select your code, use the Ctrl +Shift + P option to open the command pallet and choose the "Copy with Syntax Highlighting" option. Now when you paste the code, it should have the proper tabs and indentation, but it will have no color formatting.

    2. If you must have the color formatting then you can first set the colour theme to "light mode" from General Settings then follow the same step 1, past it into a Word document with the option "Keep Source Formatting". This will you give you the same result as the File Print option in the older CCS. 

    Thanks,

    Ira