This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM33-SDK: Issue on length configure in linker file ?

Part Number: MSPM33-SDK
Other Parts Discussed in Thread: MSPM33C321A

Hello, 

I'm working on MSPM33C321A eval board, and I use the "empty" exemple on Code Composer Studio.

When I read the linker file (device_linker.cmd) automatically generated, I see that :

MEMORY
{
    FLASH           (RX)  : origin = 0x10000000, length = 0x000FFFFF
    SRAM            (RWX) : origin = 0x30000000, length = 0x0003FFFF
    DATA            (R)   : origin = 0x80000000, length = 0x00007FFF
    BCR_CONFIG      (R)   : origin = 0x80101800, length = 0x000003FF
    BSL_CONFIG      (R)   : origin = 0x80101C00, length = 0x000003FF
}
 
Are there any errors, is it not ?
MEMORY
{
    FLASH           (RX)  : origin = 0x10000000, length = 0x000100000
    SRAM            (RWX) : origin = 0x30000000, length = 0x00040000
    DATA            (R)   : origin = 0x80000000, length = 0x00008000
    BCR_CONFIG      (R)   : origin = 0x80101800, length = 0x00000400
    BSL_CONFIG      (R)   : origin = 0x80101C00, length = 0x00000400
}
 
Thanks