Hello,
There's a problem a bit more complicated to solve, but hope someone might have an idea:
I have a Buildbot server that calls an automatic build script by a service running on a VMWare Windows 7 slave to build the project using CCSv5.1.1 which after upgrade (from CCSv5.1.0) stopped working, I'm using the C6748.GEL provided by LogicPD and created a .ccxml connection for XDS100v1. I've tried reinstalling CCSv5.1.1, also the USB drivers for VM Windows, but I have the same problem:
Loading Firmware: c:/ti/ccsv5/ccs_base/scripting/examples/loadti/loadti.bat -a -c TMS320C6748.ccxml -x ../log.xml Debug/UnitTesting.out
Configuring Debug Server for specified target... Done TARGET: Texas Instruments XDS100v1 USB Emulator_0
Connecting to target... Error code #4001, could not connect to target! Aborting!
SEVERE: ICEPICK_C: Error connecting to the target: (Error -151 @ 0x0) One of the FTDI driver functions used during the connect returned bad status or an error. The cause may one or more of: invalid emulator serial number, blank emulator EEPROM, missing FTDI drivers, faulty USB cable. Use the xds100serial command-line utility in the 'common/uscif' folder to verify the emulator can be located. (Emulation package 5.0.569.0)
SEVERE: emulation failure occurred SEVERE: Error connecting to the target: emulation failure occurred
Funny thing it works if I start it from console manually within the VM, also xds100 test reports all tests passed.
Any idea why is not working at all? Should I revert back to CCSv5.1.0 which worked but occasionally failed? Is it related to some Windows rights for services?
Thank you in advance for any suggestions,
David.