This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS v5 Debug Error XDS510PP Plus/TMS320DM642

Other Parts Discussed in Thread: TMS320DM642

Dear All,

 

  I’m new to DSP programming and I have a problem when I try to run the project debug on my Emulator/DSP. I get the error message "Error 0x80000260/-1146 from Code Composer Studio". I attached a screenshot of the error.

I use a XDS510PP Plus from Spectrum Digital. I could successfully check the emulator with the software SdConfig v3.1. Verify, Test, and Diagnostic does not give any message error. I set the parallel port as follow:

Mode: EPP

Base I/O: 378

Interrupt: IRQ 7

 

I’m using Code Composer Studio v5.1.1.00028, on a old laptop IBM Thinkpad (Pentium 4  CPU 2.8GHz, 504 MB RAM (2 GB Virtual RAM) ). I have no other computers or laptop with the parallel port (the only USB to Parallel adapter I could find is not working on this hardware). I also tried a Texas Instruments XDS100v2 USB Emulator, but cannot find the target board or device (maybe not compatible?).

 

The project setting is the follow:

Family: C6000

Variant: TMS320DM642

Connection: Spectrum Digital XDS510 Parralel Port-PCI Emulator

In target configuration file is set I selected the “Board or Device” TMS320DM642.

 

I successfully compiled the programs but I cannot run the debug.

I tried four different sample programs (My project, CCSv5 Empty project, CCSv5 Hello World, CCSv5 SYS/BIOS Tipical), both debug and release. I also re-install CCS.

 

Unfortunately I could not find solution about this error. Any help or hint will be really appreciated.

 

Thanks in advance,

Alessandro

  • I guess it's because of wrong target configuration file?

  • Dear Lucifar,

      thank you for the reply.

    I don't know exactly what it can be wrong. I left all the original configuration options.

    I use a XDS510PP Plus, but I cannot find inside the list of the possible connections. I just found "Spectrum Digital XDS510 Parallel Port-PCI Emulator", which I thought could be the target.

    I also selected "TMS320DM642" as board or device, which is my device.

    It may be possible that the CCSv5 does not have the necessary drivers?

    Regards,

    Alessandro

  • Hello Alessandro,

    Alessandro Moro said:
    I use a XDS510PP Plus, but I cannot find inside the list of the possible connections. I just found "Spectrum Digital XDS510 Parallel Port-PCI Emulator", which I thought could be the target.

    Yes that is correct.

    You are getting a connection error. Can you try using the SDConfigEx v5 utility to test your JTAG connection?

    Thanks

    ki

  • Dear Ki-Soo,

      thank you for the reply. I tried to use SDConfigEx v5 utility, but I did not get any error (I tried the options Configuration->Verify, Emulator->Test, Emulator->Diagnostics).

    I attached the output screenshots with the hope they will be helpful.

    Best Regards,

    Alessandro

  • Dear All,

       thank you for your help. Unfortunately I was not able to solve my problems with THAT emulator-dsp configuration. I was not able to figure out which could be the reason.

    I get a new emulator (Blackhawk XDS560v2) to use with my DSP. However, if the emulator is perfectly working, I could not work with the DSP (DM642). This is the procedure I followed:

    "Blackhawk Control Panel (32-bit)", and no errors were detected (attached file).

    I tried to run a simple "Hello world" program with Code Composer Studio v5.1.1.00031.
    I set the target configuration as follow:

    Connection: Blackhawk XDS560v2-USB System Trace Emulator

    Board or Device: TMS320DM642

    and when I tested I got this message:


    [Start]

    Execute the command:

    %ccs_base%/common/uscif/

    dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity

    [Result]


    -----[Print the reset-command software log-file]-----------------------------

    This utility has selected a 560-class product.
    This utility will load the program 'bh560v2u.out'.
    The library build date was 'Dec 19 2011'.
    The library build time was '21:41:44'.
    The library package version is '5.0.569.0'.
    The library component version is '35.34.39.0'.
    The controller does not use a programmable FPGA.
    The controller has a version number of '5' (0x00000005).
    The controller has an insertion length of '0' (0x00000000).
    The cable+pod has a version number of '8' (0x00000008).
    The cable+pod has a capability number of '7423' (0x00001cff).
    This utility will now attempt to reset the controller.
    This utility has successfully reset the controller.

    -----[Print the reset-command hardware log-file]-----------------------------

    The scan-path will be reset by toggling the JTAG TRST signal.
    The controller is the Nano-TBC VHDL.
    The link is a 560-class second-generation-560 cable.
    The software is configured for Nano-TBC VHDL features.
    The controller will be software reset via its registers.
    The controller has a logic ONE on its EMU[0] input pin.
    The controller has a logic ONE on its EMU[1] input pin.
    The controller will use falling-edge timing on output pins.
    The controller cannot control the timing on input pins.
    The scan-path link-delay has been set to exactly '2' (0x0002).
    The utility logic has not previously detected a power-loss.
    The utility logic is not currently detecting a power-loss.

    -----[The log-file for the JTAG TCLK output generated from the PLL]----------

      Test  Size   Coord      MHz    Flag  Result       Description
      ~~~~  ~~~~  ~~~~~~~  ~~~~~~~~  ~~~~  ~~~~~~~~~~~  ~~~~~~~~~~~~~~~~~~~
        1   none  - 01 00  500.0kHz   -    similar      isit internal clock
        2   none  - 01 09  570.3kHz   -    similar      isit internal clock
        3    512  - 01 00  500.0kHz   O    good value   measure path length
        4    128  - 01 00  500.0kHz   O    good value   auto step initial
        5    128  - 01 0D  601.6kHz   O    good value   auto step delta
        6    128  - 01 1C  718.8kHz   O    good value   auto step delta
        7    128  - 01 2E  859.4kHz   O    good value   auto step delta
        8    128  + 00 02  1.031MHz   O    good value   auto step delta
        9    128  + 00 0F  1.234MHz   O    good value   auto step delta
       10    128  + 00 1F  1.484MHz   O    good value   auto step delta
       11    128  + 00 32  1.781MHz   O    good value   auto step delta
       12    128  + 01 04  2.125MHz   O    good value   auto step delta
       13    128  + 01 11  2.531MHz   O    good value   auto step delta
       14    128  + 01 21  3.031MHz   O    good value   auto step delta
       15    128  + 01 34  3.625MHz   O    good value   auto step delta
       16    128  + 02 05  4.313MHz   O    good value   auto step delta
       17    128  + 02 13  5.188MHz   O    good value   auto step delta
       18    128  + 02 23  6.188MHz   O    good value   auto step delta
       19    128  + 02 37  7.438MHz   O    good value   auto step delta
       20    128  + 03 07  8.875MHz   O    good value   auto step delta
       21    128  + 03 15  10.63MHz   O    good value   auto step delta
       22    128  + 03 1E  11.75MHz  {O}   good value   auto step delta
       23    512  + 02 3E  7.875MHz   O    good value   auto power initial
       24    512  + 03 0E  9.750MHz   O    good value   auto power delta
       25    512  + 03 16  10.75MHz   O    good value   auto power delta
       26    512  + 03 1A  11.25MHz   O    good value   auto power delta
       27    512  + 03 1C  11.50MHz   O    good value   auto power delta
       28    512  + 03 1D  11.63MHz   O    good value   auto power delta
       29    512  + 03 1D  11.63MHz   O    good value   auto power delta
       30    512  + 03 13  10.38MHz  {O}   good value   auto margin initial

    The first internal/external clock test resuts are:
    The expect frequency was 500000Hz.
    The actual frequency was 499110Hz.
    The delta frequency was 890Hz.

    The second internal/external clock test resuts are:
    The expect frequency was 570312Hz.
    The actual frequency was 569976Hz.
    The delta frequency was 336Hz.

    In the scan-path tests:
    The test length was 16384 bits.
    The JTAG IR length was 38 bits.
    The JTAG DR length was 1 bits.

    The IR/DR scan-path tests used 30 frequencies.
    The IR/DR scan-path tests used 500.0kHz as the initial frequency.
    The IR/DR scan-path tests used 11.75MHz as the highest frequency.
    The IR/DR scan-path tests used 10.38MHz as the final frequency.

    -----[Measure the source and frequency of the final JTAG TCLKR input]--------

    The frequency of the JTAG TCLKR input is measured as 10.37MHz.

    The frequency of the JTAG TCLKR input and TCLKO output signals are similar.
    The target system likely uses the TCLKO output from the emulator PLL.

    -----[Perform the standard path-length test on the JTAG IR and DR]-----------

    This path-length test uses blocks of 512 32-bit words.

    The test for the JTAG IR instruction path-length succeeded.
    The JTAG IR instruction path-length is 38 bits.

    The test for the JTAG DR bypass path-length succeeded.
    The JTAG DR bypass path-length is 1 bits.

    -----[Perform the Integrity scan-test on the JTAG IR]------------------------

    This test will use blocks of 512 32-bit words.
    This test will be applied just once.

    Do a test using 0xFFFFFFFF.
    Scan tests: 1, skipped: 0, failed: 0
    Do a test using 0x00000000.
    Scan tests: 2, skipped: 0, failed: 0
    Do a test using 0xFE03E0E2.
    Scan tests: 3, skipped: 0, failed: 0
    Do a test using 0x01FC1F1D.
    Scan tests: 4, skipped: 0, failed: 0
    Do a test using 0x5533CCAA.
    Scan tests: 5, skipped: 0, failed: 0
    Do a test using 0xAACC3355.
    Scan tests: 6, skipped: 0, failed: 0
    All of the values were scanned correctly.

    The JTAG IR Integrity scan-test has succeeded.

    -----[Perform the Integrity scan-test on the JTAG DR]------------------------

    This test will use blocks of 512 32-bit words.
    This test will be applied just once.

    Do a test using 0xFFFFFFFF.
    Scan tests: 1, skipped: 0, failed: 0
    Do a test using 0x00000000.
    Scan tests: 2, skipped: 0, failed: 0
    Do a test using 0xFE03E0E2.
    Scan tests: 3, skipped: 0, failed: 0
    Do a test using 0x01FC1F1D.
    Scan tests: 4, skipped: 0, failed: 0
    Do a test using 0x5533CCAA.
    Scan tests: 5, skipped: 0, failed: 0
    Do a test using 0xAACC3355.
    Scan tests: 6, skipped: 0, failed: 0
    All of the values were scanned correctly.

    The JTAG DR Integrity scan-test has succeeded.

    [End]




    After that, I tried to run the program debug to test the code, but without success. The compiler returned this message error:

    C64x: Error connecting to the target: (Error -234 @ 0x0) The instruction scan-path cannot circulate bits, it may be broken. An attempt to scan the JTAG instruction registers has failed. The target's JTAG instruction path appears to be broken with a stuck-at-ones or stuck-at-zero fault. (Emulation package 5.0.520.0) .
    Now I'm using the emulator with a DM642 Evaluation Module with success, but I have a different problem (maybe better to open a different topic).
    Thank You in advance for any help.
    I will post the solution (if I will be able to find).
    Regards,
    Alessandro