Part Number: CC2745R10-CS-EVM-DOC-CERT
I am considering trying out the samples included with the CC2745 LaunchPad and the SDK, “SimpleLink SDK Edge AI Plugin.”
I checked the README for the SDK samples, but it appears that all of the samples are configured to use a BoosterPack.
Therefore, I would like to ask whether there are any Edge AI samples that can be used with only the LaunchPad, without using a BoosterPack.
Alternatively, are there any samples or application notes for using Edge AI with the CC2745?
I am still not quite sure how to use Edge AI with the CC2745, so I apologize if my question is misguided.
Best regards,