This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to interpret difference in binary built from same environment

I was working on an issue in OMAP4 Multimedia and noted that the issue is  fixed by ONE of these

-          Addition of a log, just add it and build, no need to capture logs at runtime

-          Do a fresh download of the code and build

-          Move to a new version of codec

-          Enable level 5 ducati logs

 

This suggested that the issue is with the build. I confirmed that the build environment – the folder location, clean build, no code differences, location of tools, build commands – are all the same.

But, still find issue reproduced with binaries built in my original folder.

 

Having not aware of ways to compare the resultant binary I am approaching you.

I have shared the baseimage and its map files for OK and NG case here \\cnx0053806\For_Analysis\ (TI Internal Network)

Please suggest.

 

The tools used are :

Codec Engine  : 3.20.00.08

Framework Components : 3.20.00.12.eng

XDAIS  : 7.20.00.01.eng

OSAL  : 1.20.00.06.eng

BIOS  : 6.31.03.25

XDC Tools  : 3.20.07.86

CG Tools  : 4.6.1

OS: Linux

Ducati Release : 1.23-P2