Hi there,
I'm seeing following error when I test JATG interface. Could you please let me know what would have been wrong?
Please let me know if you need any info.
CCS version: ccv v5
JATG: BH-USB-560BP
Board: panda 4430
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 560-class product.
This utility will load the program 'bh560ubp.out'.
E_RPCENV_IO_ERROR(-6) No connection: Client has disconnected
Failed to open i/o connection (bh560ubp:0)
An error occurred while soft opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-250' (0xffffff06).
The title is 'SC_ERR_ECOM_EMUNAME'.
The explanation is:
An attempt to access the named emulator via USCIF ECOM has failed.
Thanks & Regards,
Venkat