Dear ladies and gentlemen,
I am trying to use Matlab Simulink mit CCSLINK for a Texas Instruments DSP using Code Composer Studio 3.3.
Since Code Composer Studio needs Administrator Rights (for Windows Vista), I am logged in as an administrator.
When starting Code Composer Studio “standalone”, I explicitly call it “as administrator” and it works fine.
When trying to connect to Code Composer Studio via Matlab Simulink with CCSLink by typing
cc = ticcs
I receive the error message:
“Error reading Code Composer Setup information. Code Composer may not have been correctly installed”.
The same error occurs if I am trying to start CCS “standalone” (even when logged in as administrator) without explicitly doing it “as administrator”.
I assume, that Matlab/CCSLink will not explicitly be trying to start CCS “as administrator”.
Is there a workaround for this issue? I assume anyone who is using CCS 3.3 with Matlab Simulink CCSLink on a Windows Vista machine may come around the same problem.
Thank for you comments/ideas/support.