CCSTUDIO-THEIA: AI assistant base URL issue

Part Number: CCSTUDIO-THEIA

Hi,

I want to use AI assistant with codex inside CCS 21.0.1

For security reasons, the IT department has blocked direct access to chatGPT and I have to use an intermediate provider.
I configured this in Base URL field of AI assistant settings like this

but I get the following answer


IT department have checked traffic logs from my PC and all my requests are directed to chatGPT and not to our provider as if the Base URL configuration has no effect.
For a test purpose IT have temporarily allowed access to chatGPT and I get valid answer with still the same config in CCS, so this confirm that my requests are sent to chatGPT and not to our provider.

To be sure I also do a test in windows terminal with the following command :

curl.exe -H "Authorization: Bearer **********************" -H "Content-Type: application/json" https://oai-t-foundry-agentai.openai.azure.com/openai/v1/responses -d "{\"model\":\"gpt-5.3-codex\",\"input\":\"hello\"}"

and I get valid answer, so my access to our provider is well working and the issue is only with CCS.

I have a similar issue with claude and I'm also not able to use it

Do you have solution to allow me to use codex?

Regards