Part Number: UNIFLASH
I am trying to flash the CC2340R22 chip on a custom board using DSLite/the Uniflash CLI. However, when running the command
C:\\ti\\uniflash_9.6.0\\dslite.bat --mode noConnectFlash --config=C:\\ti\\uniflash_9.6.0\\XDS0002.ccxml --flash <hex file path>
XDS0002.txt Changed the .ccxml file to a .txt file so I could attach it here.
It will throw the Error -615 "incorrectly formatted SWD".
Without touching the board, the connections, or the XDS110, I will then open Uniflash and I am able to flash the exact same file to the board using the GUI.
Then when trying to flash using CLI it fails with the same error.
Is there some CLI command I am missing to make it work?