Hi,
In CCS 5, when an error or warning occurs during build, the relevant error message in the build console is highlighted in red or yellow respectively. The message can also be double-clicked, to quickly jump to the offending line in the source code.
However, the line that is actually highlighted is always the one below the line where the error message appears. This is very confusing and annoying and sometimes prevents being able to double-click the line at all (as sometimes the highlighted line happens to be empty, and you must double click on actual text for the double-click to be recognized).
If I recall correctly this problem in some form or another dates back as far as CCS 2. Is there any chance it will ever be fixed?
-itay