Part Number: CCSTUDIO-THEIA
I am currently using CCS Version: 21.0.1.10__1.12.1.
I am using an external library (WIZnet).
I don't understand how to specify the additional include path for it.
I do know that I need to add it via this screen, though.

For a single source file (e.g, main.c), I can add it by selecting the filename and right-clicking to select [Properties...].
However, I don't know of a reliable way to add this to all source files (*.c).
A related issue is that include specifications do not take effect when the "-Iquote" option is used.
The build log showed the string "-Iquote xxxx", but it was not enabled (specified with double quotes "").
Specifying with "-I" is valid.
Best regrads.