Part Number: CCSTUDIO-THEIA
I am currently using CCS Version: 21.0.1.10__1.12.1 (Windows).
I have the following folder structure:
(work root)\
|--ProductA\
| |--- Doc (Documnet)
| |--- Inf (Reference information)
| \--- ProjA (Workspace)
|--ProductB\
| |--- Doc (Documnet)
| |--- Inf (Reference information)
| \--- ProjB (Workspace)
|--ProductC\
| |--- Doc (Documnet)
| |--- Inf (Reference information)
| \--- ProjC (Workspace)
.....
In such a case, what is the proper way to create a new ProjXX?
Currently, I am working on the following steps:
1. Create ProjXX in the current folder (within CCS).
2. Move ProjXX to the desired location (folder) (using Windows Explorer).
There are two related issues.
1. How can I open ProjA directly?
How can I open ProjA directly from Windows Explorer?
Currently, I've associated CSS with a folder and launch CSS by right-clicking (Shift+) on the folder.
2. What is the proper way to rename a project?
For example, ProjA --> ProjD
Currently, I open the parent folder in CCS and renaming it there.
Best regards,
Kato T.