This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
My intention is to migrate a C6747 project from CCSv3.3 to CCSv5.1
I am using an OMAP-L137/TMS320C6747 evaluation board and the Spectrum Digital EVMOMAP_L137 onboard USB Emulator. Also, I use a CCS v5.1 90-day evaluation license.
I built and tested a sample project in CCS V3.3 IDE, and then the working project was imported into CCSv5.1. I can build the project without errors in the CCSv5.1 Edit mode, but I failed to launch the debug session – the CCS got into infinite loop in launching project.
My CCSV5 configuration settings are: Connection – Spectrum Digital DSK-EVM PLUS onboard USB Emulator; Board or Device – EVMOMAPL137; initialization script - evmomapl137_dsp.gel
I would appreciate your help to fix this problem.
Hello,
appologies as this post seems to have slipped through the cracks. Let me see if we can try to help you here.
How did you import the project? What do you mean by "CCS got into infinite loop" ? What exactly are you experiencing? Do you see any errors? Are there any error logs or dump (.dmp) files?
Best Regards,
Lisa