This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

"Connect CCS 5 to TMDXSCBP6618X."

Other Parts Discussed in Thread: TMS320C6670

 
Hi
 
I am unable to connect the CCsv5 with SCBP board " TMDXSCBP6618X "  consisting of TMS320C6618 processor.
 
For the example project "Hello World", I am not able to create debug session. Whenever, I tried launching debug session,
Following error is displayed:
 
"""""unable to communicate with the emulator
check the target configuration or reset the the emulator and check the emulator configuration  """"
 
Target configuration file is created as per emulator connections.
Settings used for making target configuration file:
 
Connection:USB560-M emulator
Device:TMS320C6670
core 66x
 
 
My objective is to write code as per project requirements, compile and flash into the TMS320C6618 processor on the TMDXSCBP6618X board.
  • Hello,

    Vivek Khanna said:
    """""unable to communicate with the emulator
    check the target configuration or reset the the emulator and check the emulator configuration  """"

    Can you check to see if your PC has proper communication with your emulator? Run the 'Blackhawk Control Panel' that comes with CCSv5 and see if your USB560M is detected and there are valid values for the Serial Number and HW/Firmware revision numbers.

    ki