Hi,
I'm currently looking to use a TMS320C6713 DSP Starter Kit for a school project. I'm abit confused as to why the TI estore states that it comes with CCS v2.2, whereas other sources I refer to states that it comes with CCS v5. Anyway, my main concern is whether CCS v5 is fully compatible with the Embedded Coder function in Matlab (2011 or 2012 version)? I tried looking into other sites, but the closest info that I could find was that the Embedded Coder is not really compatible with CCS v4 without the use of the XMakefile utility. Can anyone help me with this?