This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How to add emulator support in CCSv5 without re-installing the whole software?

I only selected Spectrum Digital emulator support when I installed CCS v5, how can I install the other drivers without re-installing CCS v5 again and losing the settings I worked so hard on?

  • Hello,

    you should be able to re-run the installer and add features.  Just point it to the same CCS installation and it should detect the installation and go from there.

    Please keep us informed.

    Best Regards,

    Lisa

  • Hi Lisa,

    Thanks, it worked for Code Composer Studio v6 with Windows 7, 64-bit, emulator Spectrum Digital XDS510 USB.. However I'm now getting

    Unable to load ..\..\..\emulation\tpi\tpi28xx.dll: The application has failed to start because its side-by-side configuration is incorrect. Please see the application event log or use the command-line sxstrace.exe tool for more detail.

    I will check other threads for a solution.

    Greg