This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C2000 compiler with MISRA enabled

I have downloaded the 6.02 version of the code generator and am running with MISRA checking enabled.  However there are include files from the compiler itself as well as those from the control suite that are not MISRA clean.  Is there a set of include files that comply with all of the MISRA rules?

Thanks

 

  • Ian,

    At the moment, the include files provided with the compiler tools are not MISRA compliant. Please see this related thread whcih mentions an enhancement request we have in place to track this request. Note, as per the last response in that thread, that there are no immediate/short-term plans to do this but may be something we do in the future.