All:
CCS Version: 5.1.0.09000
Sometimes, when I load code into the C5505 via XDS100v2, the emulator does NOT go to "main," as is normal. It downloads, and looks like it the processor is running. I can halt, reset, and restart, and that will allow it to go to "main."
This is an infrequent occurance, but it is bothersome - I have no idea what the processor could be doing. This is happening on a custom target board.
I have also worked with the EVM5515, and using the embedded emulation, I did not see even one time where the C5515 exhibited the same behavior.
Regards,
Todd Anderson