Hi,
I have downloaded CCS5.1.1.00031 and installed. When i connect to eval board with XDS 510 USB emulator
license problem coming. is there any solution for this ?
Regards
Vadivel
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have downloaded CCS5.1.1.00031 and installed. When i connect to eval board with XDS 510 USB emulator
license problem coming. is there any solution for this ?
Regards
Vadivel
Hi Vadivel,
what type of license do you have/plan to use? What error do you see? What is your current setup?
Please see this wiki for the supported license setups.
http://processors.wiki.ti.com/index.php/Licensing_-_CCS
Best Regards,
LIsa
I've run into the same problem. I believe with my evaluation 90 day license, the XDS510 is not supported until I upgrade to a full version.
However, It would be nice if the "Test Connection" feature of the configuration tool would mention that the evaluation version is limited.
Instead I get this output
[Start]
Execute the command:
%ccs_base%/emulation/drivers/sdjtag.exe -f %boarddatafile% -v -X reset -X scantest
[Result]
** BoardFilePath: C:\Users\alynch\AppData\Local\.TI\2825812290\0\0\BrdDat\testBoard.dat
** Resetting Emulator
-- Emulator is Reset
** Emulator Scan Test
ERROR -- XDS510-USB Emulator not connected/enumerated[End]
I used the free limited licence for my 6678 evm. When I tried to set up the target configuration, I can not find the xds100v1 option in connection type. P.S. I installed the CCSv5.2 which should include the xds100 driver. Thank you.