I'm using "C6000 Code Generation Tools 7.3.2"
I'd like to report a documentation error/bug. The following is misleading and erroneous.
6.9.2 The CLINK Pragma
The CLINK pragma can be applied to a code or data symbol. It causes a .clink directive to be generated
into the section that contains the definition of the symbol. The .clink directive indicates to the linker that the
section is eligible for removal during conditional linking. Therefore, if the section is not referenced by any
other section in the application that is being compiled and linked, it will not be included in the output file
result of the link.
The syntax of the pragma in C/C++ is:
#pragma CLINK (symbol )
I had to find the real answer from this thread:
http://e2e.ti.com/support/development_tools/compiler/f/343/t/136174.aspx
-----------------------------------------------------------------------------------------------------------------------