Hello,
i have a problem with Code Composer Studio v5.1.1.00031 runningon a Win7 x64 System:
I´m using an Olimex MSP430 Board (MSP-5438STK) and an MSP430-JTAG-ISO-Adapter from Olimex.
Installation of CCS and JTAG-drivers was fine - no problems.
Build of example-project without errors. When I start "Debug" the project, i get the error-message:
"Error connecting to the target: Could not find device (or device not supported)".
A click on the "retry"-Button and it works - the compiled code is written to the MSP and debugging is possible.
So far, is it possible to work - but when I "Terminate" the Debug-Session, the CCS crashs without any further information.
I think there is a problem between CCS and the JTAG-Adapter, but i don´t know how to fix it.
CCS is new for me, maybe there is a simple checkbox or an option to activate and solve the problem.
Thank you for your help.