Other Parts Discussed in Thread: CCSTUDIO
All:
I have been using the CCS 5 to show really nice pictures of waveforms. I have up to 8000 32-bit numbers, 2's compliment, and it does a very good job - when it works.
Typically, I will display the waveform, then make a code change, and then re-run to see what impact my change has on the waveform. I halt the emulator to display what is captured in the 8000-deep buffer. This data is put into the buffer during an interrupt service routine.
MANY times I get to the point of displaying a waveform, and "Tools-->Graph-->" will give me grayed out options. I can usually get around this by reloading and rerunning the code. However, there are times when I need to shut down CCS5 and bring it back up to get to display a waveform - which can be very frustrating!
Is there a setting that I am missing? Perhaps a gel-file setting? A CCS 5 setting?
I am running a c5505 processor on a target board, attaching via XDS100 emulator.
Having the graphing capability has been a GOOD thing. Having all of the problems with it is not.
Regards,
Todd Anderson