Hi Champ,
I'm trying to connect xds100v2(Rev. B) to DM365EVM(Rev. E) with CCS v5.1.100031. But I got error massages below when I launch the target configration and connect it.
So, could you please let me know how I can connect the emulator to the EVM?
-- In Console tab ----------------------------------------------------------------------------
ARM9: GEL Output:
DM365EVM ARM Startup Sequence
ARM9: GEL Output: VPSS Sync Reset Fix
ARM9: GEL: Error while executing OnTargetConnect(): Target failed to write memory at 0x01C21C0C at *((unsigned int *) 0x01C21C0C)=0x00020002
[evmdm365.gel:103] at OnTargetConnect() .
ARM9: Error: (Error -1060 @ 0x2E18) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.0.569.0)
ARM9: Error: (Error -1029 @ 0x2B5F) Invalid data read from ICECrusher register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.0.569.0)
----------------------------------------------------------------------------------------------------
Thanks in advance for your cooperation.
Best regards,
Kohei Shikama