I have the following configuration:
Windows 7
CCSv5 (5.1.0.09000)
emulator: XDS510PP+
target: TMS320F2810
I can't get the emulator to work. I set it up using the Target Configuration option to have the right emulator and target (although it lists the XDS510PP, it doesn't list the +). But when I try to launch the selected configuration, it fails with a "Disconnected: Unknown" message.
I also tried using the utility SdConfigEx.exe to debug the problem. When I use it to scan the ports (Configuration > Ports Available > Printer, USB), it gives the error message "Could not open the driver (.sys file)". From what I've read, the emulator driver should have been installed when CCS was installed. I can't find a driver for the emulator that supports CCSv5 on the internet, so I'm at a loss.