This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Suggestions for creating CCS V5.1 workspaces/projects to work within SVN source control

Other Parts Discussed in Thread: CCSTUDIO

Our team is upgrading from CCS 3.3 to CCS 5.1  We are quite familiar with 3.3 but the organization of eclipse and CCS 5.1 is quite different.  Can you suggest or point me to some documentation of best practices for setting up workspaces and projects that are to be shared by our team in SVN?

Here are some specific issues we're trying to address:

1. CCS 5.1 asks us to create a workspace.  Should we only create one?  It seems to want to put it in the "My Documents" folder.  Why is that the default?  Can we put it in the C:\ti folder with all the other CCS 5.1 stuff?  This would be similar to v3.3 where there was a "My Projects" folder under the ccs3.3 install folder.

2. Each developer will have their own workspace folder.  Do we than check-out projects from SVN and store them in all in the workspace folder?  Or do we create sub-folders and put the projects in the sub-folders?  Or will CCS 5.1 do this for us automatically.

thanks,

Mike

  • Hi Mike,

    First off, some helpful resources to read:

    http://software-dl.ti.com/dsps/dsps_public_sw/sdo_ccstudio/presentations/CCSv5_Tips_&_Tricks.pdf

    Specifically see slides on:

    Workspaces (slides 4-6)

    Version Control: (slide 33)

    E2E_display_name_Mike said:
    1. CCS 5.1 asks us to create a workspace.  Should we only create one?

    You can have as many as you like. Sometimes the more the better. The slides above explain why

    E2E_display_name_Mike said:
    It seems to want to put it in the "My Documents" folder.  Why is that the default?

    Don't have a definitive answer for that but I will assume because it is the main personal folder for the user. Basically it is a good idea for each user (defined by 'login' in this case) to have their own workspace folder (for the reasons described in the above slides). Hence the default is to have it in the current user's personal My Documents folder, instead of a fixed location like C:\ti, which would be the same folder for everyone

    E2E_display_name_Mike said:
     Can we put it in the C:\ti folder with all the other CCS 5.1 stuff?

    Sure. I do.

    E2E_display_name_Mike said:
    Do we than check-out projects from SVN and store them in all in the workspace folder?  Or do we create sub-folders and put the projects in the sub-folders?  Or will CCS 5.1 do this for us automatically.

    The project folder can exist inside or outside the workspace folder. If you create a project and put it inside the workspace folder, CCS will automatically create a project subfolder of the same name as the project. That project subfolder is often referred to as the 'project folder'. You would check in that project folder along with the recommended project metadata files as mentioned in the above slides.

    Hope this helps

    ki

  • Thank-you for the responses.  They are helpful.  The link you provided doesn't work (I get the Error 404).  Can you check the link?  I'd very much like the PDF.  Then I can verify your answers.

    Mike

  • Try cutting and pasting this url:

    http://software-dl.ti.com/dsps/dsps_public_sw/sdo_ccstudio/presentations/CCSv5_Tips_&_Tricks.pdf