This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cannot connect license server system



Hello,

we're running several flexlm-servers (all windowsserver2003) for a number of applications. I made a download of current lmgrd.exe + tidspssw.exe and added a new service for  CCS. Logfile is without error, but unfortunally there is a problem to access the licenses. an additional indicator is an error using lmstat-command.

  • C:\Application\CCS>lmutil lmstat -A -c ccs_license.lic
  •  lmutil - Copyright (c) 1989-2012 Flexera Software LLC. All Rights Reserved.
  • Flexible License Manager status on Mon 3/26/2012 16:01
  •  [Detecting lmgrd processes...]
  • License server status: 27000@app-aug-lic04
  • License file(s) on app-aug-lic04: C:\Application\CCS\CCS_license.lic:
  •  app-aug-lic04: license server UP (MASTER) v11.10
  •  Vendor daemon status (on app-aug-lic04):
  •  tidspssw: Cannot connect to license server system. (-15,10:10049 "WinSock: Invalid address")

I appreciate any advice to solve the problem

  • Hi Uwe,

    can you provide a few more details?

    Are you sure the port is free and not blocked by a firewall?  Have you tried using the fully resolved IP/host name? Did you follow the instructions here

    http://processors.wiki.ti.com/index.php/License_Server_Administration_for_CCS

    Best Regards,
    Lisa

  • HI Uwe,

    just thought I would check whether there is an update to your enquiry and whether the tip/wiki was helpful or if further details regarding the issue could be provided?

    Best Regards,
    Lisa