Other Parts Discussed in Thread: SYSBIOS
I am using CCS5.1.1. I have the captureVip test program running on the VPSS of the DM8168. Can I se the system analyzer to monitor CPU utilization and sysbios objects. If so, what are the steps involved in creating a project so that the system analyzer will work?
I have set up my project as a C project, just so I can browse the source. Does the project have to be RTSC-enabled?