This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
I am trying to help my customer develop a Firmware update mechanism based "loosely"on the bootloader but one where the current code can keep running while receiving the new code (firmware). We are using the F5438 experimentors board for this work and would like to be running from Flash Bank 2 while receiving code into Flash Bank 3, then switch the Vector table over when all the code is received.
My problem is getting the Linker command file to place all the code and relevant tables into FLASH2 or FLASH3 as I can't get the .cinit section to go anywhere apart from section FLASH (starting at 0x5C00). If I change
.cinit : {} > FLASH to .cinit : {} > FLASH2
I get the Error below, any ideas how I can get around this ?
C:\ti\ccsv4\ccsv4\utils\gmake\gmake -k all
'Building target: Firmware_Upgrade.out'
'Invoking: Linker'
"C:/ti/ccsv4/ccsv4/tools/compiler/msp430/bin/cl430" -vmspx -g -O0 --define=__MSP430F5438A__ --diag_warning=225 --code_model=large --silicon_errata=CPU22 --silicon_errata=CPU21 --silicon_errata=CPU23 --silicon_errata=CPU40 --printf_support=minimal -z -m"Firmware_Upgrade.map" --stack_size=160 --heap_size=160 --use_hw_mpy=F5 --warn_sections -i"C:/ti/ccsv4/ccsv4/msp430/include" -i"C:/ti/ccsv4/ccsv4/tools/compiler/msp430/lib" -i"C:/ti/ccsv4/ccsv4/tools/compiler/msp430/include" --reread_libs --rom_model -o "Firmware_Upgrade.out" "./main.obj" "./BSL.obj" -l"libc.a" "../lnk_msp430f5438a.cmd"
<Linking>
"./autoinit.c", line 30 (approximate): warning: relocation from function
"_auto_init" to symbol "__cinit__" overflowed; the 17-bit relocated address
0x1028a is too large to encode in the 16-bit field (type = 'R_MSP_REL16'
(161), file =
"C:\ti\ccsv4\ccsv4\tools\compiler\msp430\lib\rts430x.lib<autoinit.obj>",
offset = 0x00000004, section = ".text:_auto_init")
"./autoinit.c", line 30 (approximate): warning: relocation from function
"_auto_init" to symbol "__cinit__" overflowed; the 17-bit relocated address
0x1028a is too large to encode in the 16-bit field (type = 'R_MSP_REL16'
(161), file =
"C:\ti\ccsv4\ccsv4\tools\compiler\msp430\lib\rts430x.lib<autoinit.obj>",
offset = 0x0000000e, section = ".text:_auto_init")
warning: output file "Firmware_Upgrade.out" cannot be loaded and run on a
target system
'Finished building target: Firmware_Upgrade.out'
' '
Build complete for project Firmware_Upgrade
Bob,
Forwarded your message to CCS. I am not sure they are the ones to answer this, but they should be able to point us to the correct person in the compiler group that may have an idea how to help you.
Regards,
Chris
Hi Bob,
my suggestion from the error message shown above is the problem caused due to the fact that the C initialization function of the RTS (Run-Time-Support) library is compiled with small memory model which uses 16 bit pointer. When you put the .cinit section above the 64 KB address space, the RTS library can not reach it anymore. I think the workaround is to recompile the RTS library, and make a custom one. If you are using CCS v5.1, i think this should be easier for you because it comes with the Mklib tool:
http://processors.wiki.ti.com/index.php/Mklib
But let's see also what the CCS and compiler guys will tell us.
-Leo-
Hi Bob,
i just checked, actually there is already an available RTS library for this. I did the following:
- change the Runtime support library selection manually to rts430xl.lib as follows:
- and then set the data model support to large like this:
Then i modify the linker command file like you did:
.cinit : {} > FLASH2 /* INITIALIZATION TABLES */
and compilation works.
In the map file i found the following:
SECTION ALLOCATION MAP
output attributes/
section page origin length input sections
-------- ---- ---------- ---------- ----------------
.pinit 0 00005c00 00000000 UNINITIALIZED
.bss 0 00001c00 00000012 UNINITIALIZED
00001c00 00000008 rts430xl.lib : _lock.obj (.bss)
00001c08 00000008 : boot.obj (.bss)
00001c10 00000002 main.obj (.bss)
.stack 0 00005b60 000000a0 UNINITIALIZED
00005b60 00000004 rts430xl.lib : boot.obj (.stack)
00005b64 0000009c --HOLE--
.text:_isr
* 0 00005c00 0000002a
00005c00 0000002a rts430xl.lib : boot.obj (.text:_isr:_c_int00_noexit)
.text 0 00005c2a 000000b4
00005c2a 0000005c rts430xl.lib : autoinit.obj (.text:_auto_init)
00005c86 0000002a : memcpy.obj (.text:memcpy)
00005cb0 00000024 main.obj (.text:main)
00005cd4 00000004 rts430xl.lib : pre_init.obj (.text:_system_pre_init)
00005cd8 00000004 : exit.obj (.text:abort)
00005cdc 00000002 : _lock.obj (.text:_nop)
.reset 0 0000fffe 00000002
0000fffe 00000002 rts430xl.lib : boot.obj (.reset)
.cinit 0 00010000 0000000a
00010000 00000008 main.obj (.cinit)
00010008 00000002 --HOLE-- [fill = 0]
So i think this should solve the problem.
-Leo-
Hi Bob,
just another additional information.
It seems that the real problem lies on the data_model setting. You do not really need to set the rts support to rts430xl.lib manually as shown above, but instead just leave it as "automatic" per default, and set the data_model either to "restricted" or "large". I think this will automatically uses the rts library with 32(20) bit pointer and enables you to put the .cinit at memory above 64 KB.
-Leo-
Hi Chris, Leo
I am back working on this again now and I have some further questions.
I notice that run time support libs place a small amount of boot code at the very bottom of Block 0 (0x5C00) - rts430xl.lib : boot.obj
I assume this is because the reset vector is 16 bit so the code this references must be in the same 64K Block (is this correct).
But is it possible to move this into the same 512 byte segment as the Reset vector table, say at 0xFE00, so you only have to erase and program one segment in this Block.
Do I need to place all Int functions in Block 0 or is there a machanism so they can be placed in say Block 1 or Block 2 ?
Thanks
Bob Bacon
Hi
I am trying to produce some code, loosely based on the BSL, so my customer can download new firmware while the existing code is still running.
Once it has been received the vector table will be updated to point at the new code. This means the device will be twice the size required and the new code could be in any block.
But the Vector table consists of 16 bit words so is it possible to do a long jump outside the lower 64K Flash Block 0.
I have now tried this and it seems to work but I have no idea how.
For example my ".text:_isr" section is at 0x10930 but how can you jump to this from a 16 bit ISR
When I look at memory under debug it shows 0xFFFE = 0930 but how does MSP430 device select 0x10930 rather than 0x930.
Thanks
Bob Bacon
Hi Bob,
Bob Bacon said:But the Vector table consists of 16 bit words so is it possible to do a long jump outside the lower 64K Flash Block 0.
i have never tested it myself before, but i think this should be possible. Could you please try to use an "intermediate table" which mean you have another table, let's say it resides in the INFO memory. The "intermediate table" contains the 20 bit addresses, and what you do is in the normal vector table you jump first to this intermediate table, and then use the value in the intermediate table to jump to the real function. With this, i think it is then possible to jump anywhere inside the 20 bit address space.