This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Help through the connection of CCStudio and Ezdsp f2812

Other Parts Discussed in Thread: CCSTUDIO

Hi!!

 I've got some probem with my ezdspf2812, when i try to connect with the ccstudio. It's put this error: Error 0x80000200/-1135. But I don't know because a day before it's worked perfectly but now nothing.

I've try do uninstall and re-install the ccstudio but the problem can't be solved.Then i need your help for a debugging.

Thanks

  • Hello,

    Did you try running SDConfig tool to check your connection outside CCS? Are you using the on-board parallel port emulation? Also provide which CCS version you are using.

    Thanks

    ki

  • Hi!!

    Thanks for your help Ki,

    I've try running SDConfig tool but nothing then this morning i've launched SDConfig as administrator and the problem was resolved but my board continue to be very hot. After that also get another problem when running the program after loading the code in the board. It's put a message error 0x20000024/-1156 (lost processor clock, you must run in low-power mode). So i've try some another manipulation randomly and than solve the problem but my continue to be very hot.

    I'm using the on-board parallel emulation and my ccs version is V3.3

    Thanks a lot

    Fabrice

  • Fabrice,

    I do not know enough about the board to comment on if the heat being generated, if it is normal or not. It is not common for some boards to run hot. You can try checking the technical specifications and see if there is any information on temperature and such. Sorry I do not have any more suggestions.

    ki