CCS5 (5.1.0.09000)
Coded a Li-ion charger using the MSP430F2272, and it works great. In order to fully test the charger algorithm we need many cycles through different batteries, so I am using the MSP-FET tool to monitor what's going on inside the MCU.
A normal charging cycle will take a few hours. CCS5 (while in debug mode) will stop monitoring the MCU randomly, I managed to only finish one proper charging cycle without the IDE outputting this error:
"No source available for "0x0"
view disassembly (on a button)
The MCU keeps running and is alive but CCS5 disconnects the MSP-FET, which messes up the whole point of the test, which is to monitor how long it takes to charge a discharged battery.
I'm running this on windows XP SP3 but get the same error on another computer running windows 7.