And another bug i have found.
If i import a ccs3.3 project to ccs5.1, when debugging, i can not do source debugging. It always show me "No source available for "main() at...".
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
And another bug i have found.
If i import a ccs3.3 project to ccs5.1, when debugging, i can not do source debugging. It always show me "No source available for "main() at...".
Hi Xiaojun,
for this do you also have a v3.3 test project? Do you do a clean and rebuild? This message usually occurs if there are no symbols (debug information) or main function present.
Could you please provide a bit further information? Do you see this with all v3.3 projects? Do you use the Project->Import Legacy CCSv3.3 Project to import?
Best Regards,
Lisa