I use CCS5, why is On-chip flash programmer so slow, I have to wait CCS for 2 or 3minutes.
Please help me.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I use CCS5, why is On-chip flash programmer so slow, I have to wait CCS for 2 or 3minutes.
Please help me.
Hi Lisa, I use the same program,the same emulater(xds510puls). The target are both F2810. And the build option are both default setting. I think the high version(CCS5) should be faster than CCS3. CCS3 need about one minute,but CCS5 need about three minutes. Is there any other settings would affecte the speed? Best Regards, Jingjing
Hi Jingjing,
there are major differences between v3 and v5. CCSv5 is stock Eclipse based and has more features. We are aware and get constant feedback regarding the speed of CCS. You can certainly compare the build settings to see if the defaults are very different, but I do know that unfortunately CCS is not the fastest.
If this time includes debug, then you could check the emulators JTAG speed/settings.
Hope this helps clarify but I don't think there is much that can be done unfortunately.
Best Regards and all the best with development.
Lisa